Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionExtrudeCageBuilder.ContinuityType |
SubdivisionExtrudeCageBuilder.ContinuityType.SHARP
Sharp continuity
|
static SubdivisionExtrudeCageBuilder.ContinuityType |
SubdivisionExtrudeCageBuilder.ContinuityType.SMOOTH
Smooth continuity
|
Modifier and Type | Method and Description |
---|---|
SubdivisionExtrudeCageBuilder.ContinuityType |
SubdivisionExtrudeCageBuilder.continuity()
Returns the continuity.
|
static SubdivisionExtrudeCageBuilder.ContinuityType |
SubdivisionExtrudeCageBuilder.ContinuityType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionExtrudeCageBuilder.ContinuityType |
SubdivisionExtrudeCageBuilder.ContinuityType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionExtrudeCageBuilder.ContinuityType[] |
SubdivisionExtrudeCageBuilder.ContinuityType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionExtrudeCageBuilder.setContinuity(SubdivisionExtrudeCageBuilder.ContinuityType continuity)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.