Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionConnectCageBuilder.ContinuityTypes |
SubdivisionConnectCageBuilder.ContinuityTypes.SHARP |
static SubdivisionConnectCageBuilder.ContinuityTypes |
SubdivisionConnectCageBuilder.ContinuityTypes.SMOOTH |
Modifier and Type | Method and Description |
---|---|
SubdivisionConnectCageBuilder.ContinuityTypes |
SubdivisionConnectCageBuilder.continuityType()
Returns the continuity.
|
static SubdivisionConnectCageBuilder.ContinuityTypes |
SubdivisionConnectCageBuilder.ContinuityTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionConnectCageBuilder.ContinuityTypes |
SubdivisionConnectCageBuilder.ContinuityTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionConnectCageBuilder.ContinuityTypes[] |
SubdivisionConnectCageBuilder.ContinuityTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionConnectCageBuilder.setContinuityType(SubdivisionConnectCageBuilder.ContinuityTypes continuityType)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.