Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static StartSymmetricModelingBuilder.MirrorProcedureOption |
StartSymmetricModelingBuilder.MirrorProcedureOption.CUT_BODY
Deprecated.
Cuts the mesh
|
static StartSymmetricModelingBuilder.MirrorProcedureOption |
StartSymmetricModelingBuilder.MirrorProcedureOption.PROJECT_EDGE
Deprecated.
Projects the edges
|
Modifier and Type | Method and Description |
---|---|
StartSymmetricModelingBuilder.MirrorProcedureOption |
StartSymmetricModelingBuilder.mirrorProcedureOptions()
Deprecated.
Deprecated in NX10.0.0. This property is redundent and hence not necessary.
|
static StartSymmetricModelingBuilder.MirrorProcedureOption |
StartSymmetricModelingBuilder.MirrorProcedureOption.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static StartSymmetricModelingBuilder.MirrorProcedureOption |
StartSymmetricModelingBuilder.MirrorProcedureOption.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static StartSymmetricModelingBuilder.MirrorProcedureOption[] |
StartSymmetricModelingBuilder.MirrorProcedureOption.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StartSymmetricModelingBuilder.setMirrorProcedureOptions(StartSymmetricModelingBuilder.MirrorProcedureOption mirrorProcedureOptions)
Deprecated.
Deprecated in NX10.0.0. This property is redundent and hence not necessary.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.