Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.InputBodyOptions.DELETE
Delete the features
|
static MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.InputBodyOptions.HIDE
Hide the features
|
static MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.InputBodyOptions.KEEP
Keep the features as they are
|
Modifier and Type | Method and Description |
---|---|
MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.inputBodyOption()
Returns the input body option
License requirements: None. |
static MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.InputBodyOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MergeSubdivisionBodiesBuilder.InputBodyOptions |
MergeSubdivisionBodiesBuilder.InputBodyOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MergeSubdivisionBodiesBuilder.InputBodyOptions[] |
MergeSubdivisionBodiesBuilder.InputBodyOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MergeSubdivisionBodiesBuilder.setInputBodyOption(MergeSubdivisionBodiesBuilder.InputBodyOptions inputBody)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.