Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static DefineWorkRegionBuilder.WorkRegionDefinitionMethods |
DefineWorkRegionBuilder.WorkRegionDefinitionMethods.ALL
Treat all the region as work region
|
static DefineWorkRegionBuilder.WorkRegionDefinitionMethods |
DefineWorkRegionBuilder.WorkRegionDefinitionMethods.SELECTED
Specify a region as work region
|
Modifier and Type | Method and Description |
---|---|
static DefineWorkRegionBuilder.WorkRegionDefinitionMethods |
DefineWorkRegionBuilder.WorkRegionDefinitionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DefineWorkRegionBuilder.WorkRegionDefinitionMethods |
DefineWorkRegionBuilder.WorkRegionDefinitionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DefineWorkRegionBuilder.WorkRegionDefinitionMethods[] |
DefineWorkRegionBuilder.WorkRegionDefinitionMethods.values()
Returns an array that contains the values for this enum.
|
DefineWorkRegionBuilder.WorkRegionDefinitionMethods |
DefineWorkRegionBuilder.workRegionDefinitionMethod()
Returns the work region definition method
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DefineWorkRegionBuilder.setWorkRegionDefinitionMethod(DefineWorkRegionBuilder.WorkRegionDefinitionMethods workRegionDefinitionMethod)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.