Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static DefineWorkRegionBuilder.FrozenRegionDefinitionMethods |
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods.COLORED
Mark frozen region with color and do not allow its selection
|
static DefineWorkRegionBuilder.FrozenRegionDefinitionMethods |
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods.HIDDEN
Do not display the frozen region
|
Modifier and Type | Method and Description |
---|---|
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods |
DefineWorkRegionBuilder.frozenRegionDefinitionMethod()
Returns the frozen region method
License requirements: None. |
static DefineWorkRegionBuilder.FrozenRegionDefinitionMethods |
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DefineWorkRegionBuilder.FrozenRegionDefinitionMethods |
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DefineWorkRegionBuilder.FrozenRegionDefinitionMethods[] |
DefineWorkRegionBuilder.FrozenRegionDefinitionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DefineWorkRegionBuilder.setFrozenRegionDefinitionMethod(DefineWorkRegionBuilder.FrozenRegionDefinitionMethods frozenRegionDefinitionMethod)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.