Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Method and Description |
---|---|
CageSectionData |
SubdivisionBodyCollection.createEmptyCageSectionBuilder()
Creates an empty cage section builder object.
|
CageSectionData |
CageSectionDataList.findItem(int index)
Returns the object at the input index.
|
CageSectionData[] |
CageSectionDataList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CageSectionDataList.append(CageSectionData object)
Appends an object to the list
License requirements: None. |
void |
CageSectionDataList.append(CageSectionData[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CageSectionDataList.erase(CageSectionData obj)
Erases the object from the list, but does not delete the object.
|
void |
CageSectionDataList.erase(CageSectionData obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CageSectionDataList.findIndex(CageSectionData obj)
Finds the index where the input object appears.
|
void |
CageSectionDataList.insert(int location,
CageSectionData object)
Inserts an object at the specified location
License requirements: None. |
void |
CageSectionDataList.setContents(CageSectionData[] objects)
Sets the contents of the entire list.
|
void |
CageSectionDataList.swap(CageSectionData object1,
CageSectionData object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.