Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static TransverseBulkheadBuilder.Types |
TransverseBulkheadBuilder.Types.PLANES
Mold face is being defined by selected or defined planes.
|
static TransverseBulkheadBuilder.Types |
TransverseBulkheadBuilder.Types.SHEET_BODY
Mold face is being defined by a selected sheet body.
|
Modifier and Type | Method and Description |
---|---|
TransverseBulkheadBuilder.Types |
TransverseBulkheadBuilder.type()
Returns the method used to define the mold face of the transverse bulkhead.
|
static TransverseBulkheadBuilder.Types |
TransverseBulkheadBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TransverseBulkheadBuilder.Types |
TransverseBulkheadBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TransverseBulkheadBuilder.Types[] |
TransverseBulkheadBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TransverseBulkheadBuilder.setType(TransverseBulkheadBuilder.Types type)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.