Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.ALIGNED_BOUNDARY
Aligned Boundary
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.ALIGNED_LENGTH
Aligned Length
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.BOUND_TO_BOUND
Bound to Bound
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.HORIZONTAL
Horizontal
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.NORMAL_TO_CURVE
Normal to Curve
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.PARALLEL_TO_LINE
Parallel to Line
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.THROUGH_POINT
Through Point
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.VERTICAL
Vertical
|
Modifier and Type | Method and Description |
---|---|
StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.stiffenerBySupportMethod()
Returns the stiffener by support path method
License requirements: None. |
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBySupportPathBuilder.Method |
StiffenerBySupportPathBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBySupportPathBuilder.Method[] |
StiffenerBySupportPathBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StiffenerBySupportPathBuilder.setStiffenerBySupportMethod(StiffenerBySupportPathBuilder.Method method)
License requirements: nx_ship_detail ("Ship Detail Design") OR nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.