Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.CreationMethod.SPECIFY_CSYS |
static SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.CreationMethod.SPECIFY_LINE |
static SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.CreationMethod.TWO_PLANESAND_LINES |
Modifier and Type | Method and Description |
---|---|
SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.placementMethod()
Returns the placement method used to create the feature
License requirements: None. |
static SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.CreationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SteelSupportBuilder.CreationMethod |
SteelSupportBuilder.CreationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SteelSupportBuilder.CreationMethod[] |
SteelSupportBuilder.CreationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SteelSupportBuilder.setPlacementMethod(SteelSupportBuilder.CreationMethod placementMethod)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.