Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SteelSupportBuilder.CapOptions |
SteelSupportBuilder.CapOptions.NONE |
static SteelSupportBuilder.CapOptions |
SteelSupportBuilder.CapOptions.SYMMETRIC |
static SteelSupportBuilder.CapOptions |
SteelSupportBuilder.CapOptions.TWO_SIDED |
Modifier and Type | Method and Description |
---|---|
SteelSupportBuilder.CapOptions |
SteelSupportBuilder.supportCapOptions()
Returns the support cap options
License requirements: None. |
static SteelSupportBuilder.CapOptions |
SteelSupportBuilder.CapOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SteelSupportBuilder.CapOptions |
SteelSupportBuilder.CapOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SteelSupportBuilder.CapOptions[] |
SteelSupportBuilder.CapOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SteelSupportBuilder.setSupportCapOptions(SteelSupportBuilder.CapOptions supportCapOptions)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.