Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
SteelInsulationBoundaryBuilder |
SteelInsulationBuilder.createSteelInsulationBoundary()
Creates a
SteelInsulationBoundaryBuilder builder. |
SteelInsulationBoundaryBuilder |
SteelInsulationBoundaryBuilderList.findItem(int index)
Returns the object at the input index.
|
SteelInsulationBoundaryBuilder[] |
SteelInsulationBoundaryBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SteelInsulationBoundaryBuilderList.append(SteelInsulationBoundaryBuilder object)
Appends an object to the list
License requirements: None. |
void |
SteelInsulationBoundaryBuilderList.append(SteelInsulationBoundaryBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SteelInsulationBoundaryBuilderList.erase(SteelInsulationBoundaryBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SteelInsulationBoundaryBuilderList.erase(SteelInsulationBoundaryBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SteelInsulationBoundaryBuilderList.findIndex(SteelInsulationBoundaryBuilder obj)
Finds the index where the input object appears.
|
void |
SteelInsulationBoundaryBuilderList.insert(int location,
SteelInsulationBoundaryBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SteelInsulationBoundaryBuilderList.setContents(SteelInsulationBoundaryBuilder[] objects)
Sets the contents of the entire list.
|
void |
SteelInsulationBoundaryBuilderList.swap(SteelInsulationBoundaryBuilder object1,
SteelInsulationBoundaryBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.