Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SteelDistributionBuilder.SaMaterial |
SteelDistributionBuilder.SaMaterial.FIRST_VALUE |
Modifier and Type | Method and Description |
---|---|
SteelDistributionBuilder.SaMaterial |
SteelDistributionBuilder.material()
Returns the material
License requirements: None. |
static SteelDistributionBuilder.SaMaterial |
SteelDistributionBuilder.SaMaterial.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SteelDistributionBuilder.SaMaterial |
SteelDistributionBuilder.SaMaterial.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SteelDistributionBuilder.SaMaterial[] |
SteelDistributionBuilder.SaMaterial.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SteelDistributionBuilder.setMaterial(SteelDistributionBuilder.SaMaterial material)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.