Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
ShipDesignPreferencesBuilder.AngleRuleTypes.RIGHT_HAND
Angle is measured using the right hand rule system.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
ShipDesignPreferencesBuilder.AngleRuleTypes.SHIP_ORIENTATION
Angle direction and reference position is determined by the location in the ship.
|
Modifier and Type | Method and Description |
---|---|
ShipDesignPreferencesBuilder.AngleRuleTypes |
ShipDesignPreferencesBuilder.angleRule()
Returns the indication of how angles are to be measured.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
ShipDesignPreferencesBuilder.AngleRuleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes |
ShipDesignPreferencesBuilder.AngleRuleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipDesignPreferencesBuilder.AngleRuleTypes[] |
ShipDesignPreferencesBuilder.AngleRuleTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShipDesignPreferencesBuilder.setAngleRule(ShipDesignPreferencesBuilder.AngleRuleTypes angleRule)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.