Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShellTemplateBuilder.PlaneLocationTypes |
ShellTemplateBuilder.PlaneLocationTypes.EXISTING
Use existing planes to define the individual template locations.
|
static ShellTemplateBuilder.PlaneLocationTypes |
ShellTemplateBuilder.PlaneLocationTypes.OFFSET
Derive the plane locations from the orientation coordinate system or X and Y specified base planes
|
Modifier and Type | Method and Description |
---|---|
ShellTemplateBuilder.PlaneLocationTypes |
ShellTemplateBuilder.planeMethod()
Returns the value identifying how the planes (used for sections) will be specified (See
ShellTemplateBuilder.PlaneLocationTypes for the plane methods). |
static ShellTemplateBuilder.PlaneLocationTypes |
ShellTemplateBuilder.PlaneLocationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.PlaneLocationTypes |
ShellTemplateBuilder.PlaneLocationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.PlaneLocationTypes[] |
ShellTemplateBuilder.PlaneLocationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShellTemplateBuilder.setPlaneMethod(ShellTemplateBuilder.PlaneLocationTypes planeMethod)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.