Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.NONE
Do not draw template marking lines on plate.
|
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.XAND_YDIRECTIONS
Draw X and Y direction template marking lines on plate.
|
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.XDIRECTION_ONLY
Draw X direction template marking lines on plate.
|
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.YDIRECTION_ONLY
Draw Y direction template marking lines on plate.
|
Modifier and Type | Method and Description |
---|---|
ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.markingLinesDirectionType()
Returns the value that specifies which marking lines are drawn on the plate
License requirements: None. |
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShellTemplateBuilder.MarkingTypes |
ShellTemplateBuilder.MarkingTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShellTemplateBuilder.MarkingTypes[] |
ShellTemplateBuilder.MarkingTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ShellTemplateBuilder.setMarkingLinesDirectionType(ShellTemplateBuilder.MarkingTypes markingLinesDirectionType)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.