Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
SectionViewBuilder |
SectionDrawingBuilder.createSectionViewBuilder()
Creates a
SectionViewBuilder
License requirements: nx_ship_drafting ("Ship Drafting") Created in NX10.0.0 |
SectionViewBuilder |
SectionViewBuilderList.findItem(int index)
Returns the object at the input index.
|
SectionViewBuilder[] |
SectionViewBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
SectionViewBuilder |
SectionEditorBuilder.sectionView()
Returns the ship section view
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SectionViewBuilderList.append(SectionViewBuilder object)
Appends an object to the list
License requirements: None. |
void |
SectionViewBuilderList.append(SectionViewBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
SectionViewBuilderList.erase(SectionViewBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
SectionViewBuilderList.erase(SectionViewBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
SectionViewBuilderList.findIndex(SectionViewBuilder obj)
Finds the index where the input object appears.
|
void |
SectionViewBuilderList.insert(int location,
SectionViewBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
SectionViewBuilderList.setContents(SectionViewBuilder[] objects)
Sets the contents of the entire list.
|
void |
SectionViewBuilderList.swap(SectionViewBuilder object1,
SectionViewBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.