Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.SymmetricalStructureOptions.FULL
Show full section view of the bulkhead
|
static SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.SymmetricalStructureOptions.PORT
Only show port side of the bulkhead section view.
|
static SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.SymmetricalStructureOptions.STARBOARD
Only show starboard side of the bulkhead section view.
|
Modifier and Type | Method and Description |
---|---|
SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.symmetricalStructure()
Returns the symmetrical structure
License requirements: None. |
SectionViewBuilder.SymmetricalStructureOptions |
SectionEditorBuilder.symmetricalStructure()
Deprecated.
Deprecated in NX12.0.0. Use
SectionViewBuilder .SymmetricalStructure() instead.
|
static SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.SymmetricalStructureOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionViewBuilder.SymmetricalStructureOptions |
SectionViewBuilder.SymmetricalStructureOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionViewBuilder.SymmetricalStructureOptions[] |
SectionViewBuilder.SymmetricalStructureOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionViewBuilder.setSymmetricalStructure(SectionViewBuilder.SymmetricalStructureOptions symmetricalStructure)
License requirements: nx_ship_drafting ("Ship Drafting") . |
void |
SectionEditorBuilder.setSymmetricalStructure(SectionViewBuilder.SymmetricalStructureOptions symmetricalStructure)
Deprecated.
Deprecated in NX12.0.0. Use
SectionViewBuilder .SymmetricalStructure() instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.