Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SectionViewBuilder.SectionRuleOptions |
SectionViewBuilder.SectionRuleOptions.BY_RULE |
static SectionViewBuilder.SectionRuleOptions |
SectionViewBuilder.SectionRuleOptions.SIMPLE_SECTION |
Modifier and Type | Method and Description |
---|---|
SectionViewBuilder.SectionRuleOptions |
SectionViewBuilder.sectionRule()
Returns the section rule
License requirements: None. |
SectionViewBuilder.SectionRuleOptions |
SectionEditorBuilder.sectionRule()
Deprecated.
Deprecated in NX12.0.0. Use
SectionViewBuilder .SectionRule() instead.
|
static SectionViewBuilder.SectionRuleOptions |
SectionViewBuilder.SectionRuleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionViewBuilder.SectionRuleOptions |
SectionViewBuilder.SectionRuleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionViewBuilder.SectionRuleOptions[] |
SectionViewBuilder.SectionRuleOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionViewBuilder.setSectionRule(SectionViewBuilder.SectionRuleOptions sectionRule)
License requirements: nx_ship_drafting ("Ship Drafting") . |
void |
SectionEditorBuilder.setSectionRule(SectionViewBuilder.SectionRuleOptions enumSectionMethod)
Deprecated.
Deprecated in NX12.0.0. Use
SectionViewBuilder .SectionRule() instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.