Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.AF |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.DN |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.FW |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.IN |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.OT |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.P |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.S |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.UP |
Modifier and Type | Method and Description |
---|---|
SectionViewBuilder.DirectionOptions |
SectionViewBuilder.getViewDirection()
Gets the view direction
License requirements: None. |
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionViewBuilder.DirectionOptions |
SectionViewBuilder.DirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionViewBuilder.DirectionOptions[] |
SectionViewBuilder.DirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
NXObject[] |
SectionDrawingBuilder.findFocusPlates(NXObject frame,
SectionViewBuilder.DirectionOptions direction,
double offset,
double frontProximity,
double backProximity)
Returns a list of focus plates at the given position, this function is used when user want use
different frontProximity and backProximity.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.