Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static SeamBuilder.DefinitionMethods |
SeamBuilder.DefinitionMethods.CURVES_PLANES_SHIP
Can use curves, planes or other ship structure to define the seam location.
|
static SeamBuilder.DefinitionMethods |
SeamBuilder.DefinitionMethods.EQUALLY_SPACED
Create a specified number of seams equidistant between two selected curves.
|
static SeamBuilder.DefinitionMethods |
SeamBuilder.DefinitionMethods.RECTANGULAR
Create a rectangular pattern of seams based on an origin, direction, and size of rectangles.
|
Modifier and Type | Method and Description |
---|---|
SeamBuilder.DefinitionMethods |
SeamBuilder.definitionMethod()
Returns the method used to define the seam locations.
|
static SeamBuilder.DefinitionMethods |
SeamBuilder.DefinitionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamBuilder.DefinitionMethods |
SeamBuilder.DefinitionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamBuilder.DefinitionMethods[] |
SeamBuilder.DefinitionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeamBuilder.setDefinitionMethod(SeamBuilder.DefinitionMethods definitionMethod)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.