Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
ProfileCutoutBuilder.CollarPlateCreationApproaches.STEEL_FEATURE
Steel feature approach - User Collar Plate to create collar plate
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
ProfileCutoutBuilder.CollarPlateCreationApproaches.TEMPLATE
Template approach - Use Standard Part Framework to create collar plate.
|
Modifier and Type | Method and Description |
---|---|
ProfileCutoutBuilder.CollarPlateCreationApproaches |
ProfileCutoutBuilder.collarPlateCreationApproach()
Returns the approach to be used in creating collar plate.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
ProfileCutoutBuilder.CollarPlateCreationApproaches.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches |
ProfileCutoutBuilder.CollarPlateCreationApproaches.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProfileCutoutBuilder.CollarPlateCreationApproaches[] |
ProfileCutoutBuilder.CollarPlateCreationApproaches.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProfileCutoutBuilder.setCollarPlateCreationApproach(ProfileCutoutBuilder.CollarPlateCreationApproaches collarPlateCreationApproach)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.