Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.AFT_STBD_FR_OUT_CTR
Direction is Aft, Starboard, From Reference, Outside or Centered.
|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.AFT_STBD_FR_OUT_DN
Direction is Aft, Starboard, From Reference, Outside or Down.
|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.FWD_PORT_TO_IN_CTR
Direction is Forward, Port, To Reference, Inside or Centered.
|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.FWD_PORT_TO_IN_UP
Direction is Forward, Port, To Reference, Inside or Up.
|
Modifier and Type | Method and Description |
---|---|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.primary()
Returns the primary stiffener direction.
|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.primaryOnReference()
Returns the primary stiffener direction when the plate system is located on a midship reference.
|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.secondary1()
Returns the direction of the stiffener flange.
|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.secondary1OnReference()
Returns the direction of the stiffener flange when the stiffener is located on a midship reference.
|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.secondary2()
Returns the direction of the stiffener flange.
|
PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.secondary2OnReference()
Returns the direction of the stiffener flange when the stiffener is located on a midship reference.
|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateSystemBuilder.StiffenerDirectionType |
PlateSystemBuilder.StiffenerDirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateSystemBuilder.StiffenerDirectionType[] |
PlateSystemBuilder.StiffenerDirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateSystemBuilder.setPrimary(PlateSystemBuilder.StiffenerDirectionType primary)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
PlateSystemBuilder.setPrimaryOnReference(PlateSystemBuilder.StiffenerDirectionType primaryOnReference)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
PlateSystemBuilder.setSecondary1(PlateSystemBuilder.StiffenerDirectionType secondary1)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
PlateSystemBuilder.setSecondary1OnReference(PlateSystemBuilder.StiffenerDirectionType secondary1OnReference)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
PlateSystemBuilder.setSecondary2(PlateSystemBuilder.StiffenerDirectionType secondary2)
License requirements: nx_ship_basic ("Ship Basic Design") . |
void |
PlateSystemBuilder.setSecondary2OnReference(PlateSystemBuilder.StiffenerDirectionType secondary2OnReference)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.