Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PlateStockBuilder.ThickenOptions |
PlateStockBuilder.ThickenOptions.SINGLE_SIDED
Thickness is applied to only the front side of the offset mold face.
|
static PlateStockBuilder.ThickenOptions |
PlateStockBuilder.ThickenOptions.SYMMETRIC
Half of the thickness is applied to back and front sides of the offset mold face.
|
static PlateStockBuilder.ThickenOptions |
PlateStockBuilder.ThickenOptions.TWO_SIDED
The opposite thickness is applied to the back side of the offset mold face, thickness minus the opposite thickness is applied to the front side of the offset mold face.
|
Modifier and Type | Method and Description |
---|---|
PlateStockBuilder.ThickenOptions |
PlateStockBuilder.thickenOption()
Returns the thicken option.
|
static PlateStockBuilder.ThickenOptions |
PlateStockBuilder.ThickenOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlateStockBuilder.ThickenOptions |
PlateStockBuilder.ThickenOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlateStockBuilder.ThickenOptions[] |
PlateStockBuilder.ThickenOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlateStockBuilder.setThickenOption(PlateStockBuilder.ThickenOptions thickenOption)
License requirements: nx_ship_detail ("Ship Detail Design") OR nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.