Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
PlateBoundaryOptionBuilder |
PlateBuilder.createPlateBoundaryOptionBuilder()
Creates a
PlateBoundaryOptionBuilder
License requirements: nx_ship_detail ("Ship Detail Design") Created in NX11.0.0 |
PlateBoundaryOptionBuilder |
PlateBoundaryOptionBuilderList.findItem(int index)
Returns the object at the input index.
|
PlateBoundaryOptionBuilder[] |
PlateBoundaryOptionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PlateBoundaryOptionBuilderList.append(PlateBoundaryOptionBuilder object)
Appends an object to the list
License requirements: None. |
void |
PlateBoundaryOptionBuilderList.append(PlateBoundaryOptionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PlateBoundaryOptionBuilderList.erase(PlateBoundaryOptionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PlateBoundaryOptionBuilderList.erase(PlateBoundaryOptionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PlateBoundaryOptionBuilderList.findIndex(PlateBoundaryOptionBuilder obj)
Finds the index where the input object appears.
|
void |
PlateBoundaryOptionBuilderList.insert(int location,
PlateBoundaryOptionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PlateBoundaryOptionBuilderList.setContents(PlateBoundaryOptionBuilder[] objects)
Sets the contents of the entire list.
|
void |
PlateBoundaryOptionBuilderList.swap(PlateBoundaryOptionBuilder object1,
PlateBoundaryOptionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.