Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
PlaneListBuilder |
FeatureParmsBuilder.createPlaneForList()
Create a
PlaneListBuilder to add a defined
plane to a list. |
PlaneListBuilder |
PlaneListBuilderList.findItem(int index)
Returns the object at the input index.
|
PlaneListBuilder[] |
PlaneListBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PlaneListBuilderList.append(PlaneListBuilder object)
Appends an object to the list
License requirements: None. |
void |
PlaneListBuilderList.append(PlaneListBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
PlaneListBuilderList.erase(PlaneListBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
PlaneListBuilderList.erase(PlaneListBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
PlaneListBuilderList.findIndex(PlaneListBuilder obj)
Finds the index where the input object appears.
|
void |
PlaneListBuilderList.insert(int location,
PlaneListBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
PlaneListBuilderList.setContents(PlaneListBuilder[] objects)
Sets the contents of the entire list.
|
void |
PlaneListBuilderList.swap(PlaneListBuilder object1,
PlaneListBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.