Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static PillarBuilder.EndCutTypes |
PillarBuilder.EndCutTypes.NONE
No end cuts are applied
|
static PillarBuilder.EndCutTypes |
PillarBuilder.EndCutTypes.SYMMETRIC
The same end cut is applied to both ends
|
static PillarBuilder.EndCutTypes |
PillarBuilder.EndCutTypes.TWO_SIDED
Each end has different end cuts
|
Modifier and Type | Method and Description |
---|---|
PillarBuilder.EndCutTypes |
PillarBuilder.endCutType()
Returns the end cut type Symmetric or TwoSided
License requirements: None. |
static PillarBuilder.EndCutTypes |
PillarBuilder.EndCutTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PillarBuilder.EndCutTypes |
PillarBuilder.EndCutTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PillarBuilder.EndCutTypes[] |
PillarBuilder.EndCutTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PillarBuilder.setEndCutType(PillarBuilder.EndCutTypes endcutType)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.