Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
OrientationRegionItemBuilder |
OrientationDefinitionBuilder.createNewRegion(NXObject regionPoint)
Creates a new region on the landing curve to allow you to change the orientation for this area of the landing curve.
|
OrientationRegionItemBuilder[] |
OrientationDefinitionBuilder.createRegionsAtFrames()
Will create new regions at each frame.
|
OrientationRegionItemBuilder |
OrientationRegionItemBuilderList.findItem(int index)
Returns the object at the input index.
|
OrientationRegionItemBuilder[] |
OrientationRegionItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
OrientationRegionItemBuilder |
OrientationDefinitionBuilder.getNextRegion(OrientationRegionItemBuilder region)
Gets the next region to the current one.
|
OrientationRegionItemBuilder |
OrientationDefinitionBuilder.regionItemData()
Returns the regionItem builder.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationRegionItemBuilderList.append(OrientationRegionItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
OrientationRegionItemBuilderList.append(OrientationRegionItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
OrientationDefinitionBuilder.deleteRegion(OrientationRegionItemBuilder region)
Deletes a previously created region.
|
void |
OrientationRegionItemBuilderList.erase(OrientationRegionItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
OrientationRegionItemBuilderList.erase(OrientationRegionItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
OrientationRegionItemBuilderList.findIndex(OrientationRegionItemBuilder obj)
Finds the index where the input object appears.
|
OrientationRegionItemBuilder |
OrientationDefinitionBuilder.getNextRegion(OrientationRegionItemBuilder region)
Gets the next region to the current one.
|
void |
OrientationRegionItemBuilderList.insert(int location,
OrientationRegionItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
OrientationDefinitionBuilder.setAnglesNormal(OrientationRegionItemBuilder[] regions)
Will set all angle values of input regions so that web is normal to surface.
|
void |
OrientationRegionItemBuilderList.setContents(OrientationRegionItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
OrientationRegionItemBuilderList.swap(OrientationRegionItemBuilder object1,
OrientationRegionItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.