Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.ALONG_VECTOR
The web of the profile is aligned along the specified vector.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.CUBIC_TWIST
The web of the profile moves from a starting orientation to an ending orientation in a cubic fashion.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.LINEAR_TWIST
The web of the profile moves from a starting orientation to an ending orientation in a linear fashion.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.NORMAL_TO_SURFACE
The web of the profile is aligned normal to the placement surface.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.ORTHOGONAL
The web of the profile is aligned along the closest orthogonal direction to the placement surface normal.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.PLANAR_AT_ANGLE
The web of the profile is planar with respect to the defined direction.
|
Modifier and Type | Method and Description |
---|---|
OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.orientationMethod()
Returns the orientation method used to define the direction of the web for this region.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationRegionItemBuilder.OrientationMethodTypes |
OrientationRegionItemBuilder.OrientationMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationRegionItemBuilder.OrientationMethodTypes[] |
OrientationRegionItemBuilder.OrientationMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationRegionItemBuilder.setOrientationMethod(OrientationRegionItemBuilder.OrientationMethodTypes orientationMethod)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.