Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.BY_DISTANCE
The boundary is defined by a distance from a reference object.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.BY_POINT
The boundary is defined by a location on the landing curve closest to a specified point.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.FROM_END
The boundary is defined by a distance from the end of the landing curve.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.FROM_START
The boundary is defined by a distance from the start of the landing curve.
|
Modifier and Type | Method and Description |
---|---|
OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.pointMethod()
Returns the method used to define the boundary.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationPointMethodsBuilder.PointMethodTypes |
OrientationPointMethodsBuilder.PointMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationPointMethodsBuilder.PointMethodTypes[] |
OrientationPointMethodsBuilder.PointMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationPointMethodsBuilder.setPointMethod(OrientationPointMethodsBuilder.PointMethodTypes pointMethod)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.