Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationDefinitionBuilder.PlacementSideTypes |
OrientationDefinitionBuilder.PlacementSideTypes.OPPOSITE_NORMAL
The stiffener will be placed on the negative normal side of the
placement faces.
|
static OrientationDefinitionBuilder.PlacementSideTypes |
OrientationDefinitionBuilder.PlacementSideTypes.SAME_AS_NORMAL
The stiffener will be placed on the positive normal side of the
placement faces.
|
Modifier and Type | Method and Description |
---|---|
OrientationDefinitionBuilder.PlacementSideTypes |
OrientationDefinitionBuilder.placementSide()
Returns the side of the placement faces the stiffener is to be placed upon.
|
static OrientationDefinitionBuilder.PlacementSideTypes |
OrientationDefinitionBuilder.PlacementSideTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationDefinitionBuilder.PlacementSideTypes |
OrientationDefinitionBuilder.PlacementSideTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationDefinitionBuilder.PlacementSideTypes[] |
OrientationDefinitionBuilder.PlacementSideTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationDefinitionBuilder.setPlacementSide(OrientationDefinitionBuilder.PlacementSideTypes placementSide)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.