Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationDefinitionBuilder.MeasureAngleTypes |
OrientationDefinitionBuilder.MeasureAngleTypes.NORMALTO_CURVE
Angles are measured in a plane normal to the landing curve.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
OrientationDefinitionBuilder.MeasureAngleTypes.ORTHOGONAL
Angles are measured in an orthogonal plane closest to the normal of the
landing curve.
|
Modifier and Type | Method and Description |
---|---|
OrientationDefinitionBuilder.MeasureAngleTypes |
OrientationDefinitionBuilder.measureAngles()
Returns the method in which to measure angles in the orientation objects.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
OrientationDefinitionBuilder.MeasureAngleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationDefinitionBuilder.MeasureAngleTypes |
OrientationDefinitionBuilder.MeasureAngleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationDefinitionBuilder.MeasureAngleTypes[] |
OrientationDefinitionBuilder.MeasureAngleTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationDefinitionBuilder.setMeasureAngles(OrientationDefinitionBuilder.MeasureAngleTypes measureAngles)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.