Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static OrientationAngleMethodsBuilder.AlignAtTypes |
OrientationAngleMethodsBuilder.AlignAtTypes.END |
static OrientationAngleMethodsBuilder.AlignAtTypes |
OrientationAngleMethodsBuilder.AlignAtTypes.START |
Modifier and Type | Method and Description |
---|---|
OrientationAngleMethodsBuilder.AlignAtTypes |
OrientationAngleMethodsBuilder.alignAt()
Returns the indication if the region should be aligned with the adjacent region at the start of this region, or with the adjacent
region at the end of this region.
|
static OrientationAngleMethodsBuilder.AlignAtTypes |
OrientationAngleMethodsBuilder.AlignAtTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientationAngleMethodsBuilder.AlignAtTypes |
OrientationAngleMethodsBuilder.AlignAtTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientationAngleMethodsBuilder.AlignAtTypes[] |
OrientationAngleMethodsBuilder.AlignAtTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OrientationAngleMethodsBuilder.setAlignAt(OrientationAngleMethodsBuilder.AlignAtTypes alignAt)
License requirements: nx_ship_basic ("Ship Basic Design") OR nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.