Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.NeutralMethodType.BASE_LINE
Base line.
|
static InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.NeutralMethodType.CENTER_LINE
Center line.
|
static InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.NeutralMethodType.NEUTRAL_AXIS
Neutral axis.
|
Modifier and Type | Method and Description |
---|---|
InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.neutralMethod()
Returns the neutral method determines the curve that is used for measurements and calculations when un-bending the profile.
|
static InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.NeutralMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InverseBendingLinesBuilder.NeutralMethodType |
InverseBendingLinesBuilder.NeutralMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InverseBendingLinesBuilder.NeutralMethodType[] |
InverseBendingLinesBuilder.NeutralMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InverseBendingLinesBuilder.setNeutralMethod(InverseBendingLinesBuilder.NeutralMethodType neutralMethod)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.