Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static HullBuilder.Types |
HullBuilder.Types.FACES
Mold face is being defined by selected faces.
|
static HullBuilder.Types |
HullBuilder.Types.SHEET_BODY
Mold face is being defined by a selected sheet body.
|
Modifier and Type | Method and Description |
---|---|
HullBuilder.Types |
HullBuilder.type()
Returns the method used to define the mold face of the hull.
|
static HullBuilder.Types |
HullBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HullBuilder.Types |
HullBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HullBuilder.Types[] |
HullBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HullBuilder.setType(HullBuilder.Types type)
License requirements: nx_ship_basic ("Ship Basic Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.