Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ExcessMaterialBuilder.VersionID |
ExcessMaterialBuilder.VersionID.NX902
This feature builder is used to create or edit an NX902 or beyond feature.
|
static ExcessMaterialBuilder.VersionID |
ExcessMaterialBuilder.VersionID.ORIGINAL
This feature builder is used to edit an existing NX75 - NX901 excess material feature.
|
Modifier and Type | Method and Description |
---|---|
static ExcessMaterialBuilder.VersionID |
ExcessMaterialBuilder.VersionID.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcessMaterialBuilder.VersionID |
ExcessMaterialBuilder.VersionID.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcessMaterialBuilder.VersionID[] |
ExcessMaterialBuilder.VersionID.values()
Returns an array that contains the values for this enum.
|
ExcessMaterialBuilder.VersionID |
ExcessMaterialBuilder.version()
Returns the version of the feature (used to determine which properties and methods are applicable) during edit.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.