Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ExcessMaterialBuilder.Offset |
ExcessMaterialBuilder.Offset.CONSTANT
constant offset
|
static ExcessMaterialBuilder.Offset |
ExcessMaterialBuilder.Offset.LINEAR_VARYING |
Modifier and Type | Method and Description |
---|---|
ExcessMaterialBuilder.Offset |
ExcessMaterialBuilder.offsetType()
Returns the offset type (only applicable for excess material, fitup will ignore the offset type)
License requirements: None. |
static ExcessMaterialBuilder.Offset |
ExcessMaterialBuilder.Offset.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExcessMaterialBuilder.Offset |
ExcessMaterialBuilder.Offset.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExcessMaterialBuilder.Offset[] |
ExcessMaterialBuilder.Offset.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExcessMaterialBuilder.setOffsetType(ExcessMaterialBuilder.Offset offsetType)
License requirements: nx_ship_concept ("Ship Concept") OR nx_ship_mfg_prep ("Ship Manufacturing") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.