Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.COLLAR_PLATE_TO_HOLE
Check collar plate to hole
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.COLLAR_PLATE_TO_SEAM
In basic design,check collar plate to seam,In detail design,check collar plate to edge
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.CUTOUT_ANGLE
Check profile cutout angle offset
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.CUTOUT_CLEARANCE
Check cutout top and bottom clearance
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.CUTOUT_TO_HOLE
Check cutout to hole
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.CUTOUT_TO_SEAM
In basic design,check cutout to seam,In detail design,check cutout to edge
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.NUM_CHECKS
Number of check
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.PROFILE_WIDTH
Check profile width
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.STANDARD_INTERFERENCE
Check standard part interference
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.WIDE_COLLAR_PLATE
Check wide collar plate
|
Modifier and Type | Method and Description |
---|---|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExamineSteelFeatureBuilderCheck |
ExamineSteelFeatureBuilderCheck.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExamineSteelFeatureBuilderCheck[] |
ExamineSteelFeatureBuilderCheck.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ExamineSteelFeatureBuilderResult |
ExamineSteelFeatureBuilder.getCheckResult(ExamineSteelFeatureBuilderCheck check)
Get the Examining status.
|
void |
ExamineSteelFeatureBuilder.highlightCheckResult(ExamineSteelFeatureBuilderCheck check,
boolean highlight)
Highlights or unhighlights the geometries in graphic to display the check result.
|
void |
ExamineSteelFeatureBuilder.setCheck(ExamineSteelFeatureBuilderCheck check,
boolean status)
Set the flag to indicate whether or not to examine the specific object type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.