Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EndCutBuilder.SelectionTypes |
EndCutBuilder.SelectionTypes.FACE_AND_EDGE
If this Selection Type is set, then a single pair of a Face (Placement Face) and an edge(Placement Edge) needs to be specified.
|
static EndCutBuilder.SelectionTypes |
EndCutBuilder.SelectionTypes.FACES_WITH_ATTRIBUTES
If this Selection Type is set, just faces need to be specifed and placement edges will be inferred automatically.
|
Modifier and Type | Method and Description |
---|---|
EndCutBuilder.SelectionTypes |
EndCutBuilder.selectionType()
Returns the selection type.
|
static EndCutBuilder.SelectionTypes |
EndCutBuilder.SelectionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.SelectionTypes |
EndCutBuilder.SelectionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.SelectionTypes[] |
EndCutBuilder.SelectionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndCutBuilder.setSelectionType(EndCutBuilder.SelectionTypes selectionType)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.