Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static EndCutBuilder.LimitTypes |
EndCutBuilder.LimitTypes.NEAT_TRIM
If this Limit Type is set, a datum plane feature, a face or a profile/plate body needs to be selected and the endcut will be trimmed to the selected geometry.
|
static EndCutBuilder.LimitTypes |
EndCutBuilder.LimitTypes.PLANE
If this Limit Type is set, a Plane needs to be specified and the Tilt and Shear angles will be inferred from the intersection of Datum Plane with the body on which EndCut will be applied.
|
static EndCutBuilder.LimitTypes |
EndCutBuilder.LimitTypes.VALUE
If this Limit Type is set, the values of Tilt Angle and Shear Angle expressions will be used.
|
Modifier and Type | Method and Description |
---|---|
EndCutBuilder.LimitTypes |
EndCutBuilder.limitType()
Returns the limit type.
|
static EndCutBuilder.LimitTypes |
EndCutBuilder.LimitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndCutBuilder.LimitTypes |
EndCutBuilder.LimitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndCutBuilder.LimitTypes[] |
EndCutBuilder.LimitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndCutBuilder.setLimitType(EndCutBuilder.LimitTypes limitType)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.