Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
DrawingSheetBuilder |
DrawingPartBuilder.createDrawingSheetBuilder(DrawingSheet drawingSheet)
Creates a
DrawingSheetBuilder
License requirements: nx_ship_drafting ("Ship Drafting") Created in NX12.0.0 |
DrawingSheetBuilder |
SectionViewBuilder.drawingSheet()
Returns the sheet on which to create this view.
|
DrawingSheetBuilder |
DrawingSheetBuilderList.findItem(int index)
Returns the object at the input index.
|
DrawingSheetBuilder[] |
DrawingSheetBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DrawingSheetBuilderList.append(DrawingSheetBuilder object)
Appends an object to the list
License requirements: None. |
void |
DrawingSheetBuilderList.append(DrawingSheetBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DrawingSheetBuilderList.erase(DrawingSheetBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DrawingSheetBuilderList.erase(DrawingSheetBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DrawingSheetBuilderList.findIndex(DrawingSheetBuilder obj)
Finds the index where the input object appears.
|
void |
DrawingSheetBuilderList.insert(int location,
DrawingSheetBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DrawingSheetBuilderList.setContents(DrawingSheetBuilder[] objects)
Sets the contents of the entire list.
|
void |
SectionViewBuilder.setDrawingSheet(DrawingSheetBuilder drawingSheet)
License requirements: nx_ship_drafting ("Ship Drafting") . |
void |
DrawingSheetBuilderList.swap(DrawingSheetBuilder object1,
DrawingSheetBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.