Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static CustomBracketBuilder.CreationMethod |
CustomBracketBuilder.CreationMethod.PLANES_AND_POINT |
static CustomBracketBuilder.CreationMethod |
CustomBracketBuilder.CreationMethod.SPECIFY_CSYS |
Modifier and Type | Method and Description |
---|---|
CustomBracketBuilder.CreationMethod |
CustomBracketBuilder.placementType()
Returns the method used to define the placement of the bracket
License requirements: None. |
static CustomBracketBuilder.CreationMethod |
CustomBracketBuilder.CreationMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CustomBracketBuilder.CreationMethod |
CustomBracketBuilder.CreationMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CustomBracketBuilder.CreationMethod[] |
CustomBracketBuilder.CreationMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CustomBracketBuilder.setPlacementType(CustomBracketBuilder.CreationMethod placementType)
License requirements: nx_ship_concept ("Ship Concept") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.