Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static CornerCutBuilder.CutOption |
CornerCutBuilder.CutOption.CORNER
Create corner cut on selected corner point.
|
static CornerCutBuilder.CutOption |
CornerCutBuilder.CutOption.PLATE
Create corner cut for all corner points of the mold face of plate body
|
Modifier and Type | Method and Description |
---|---|
CornerCutBuilder.CutOption |
CornerCutBuilder.placementType()
Returns the type of corner cut to create.
|
static CornerCutBuilder.CutOption |
CornerCutBuilder.CutOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerCutBuilder.CutOption |
CornerCutBuilder.CutOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerCutBuilder.CutOption[] |
CornerCutBuilder.CutOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CornerCutBuilder.setPlacementType(CornerCutBuilder.CutOption cutOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.