Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Method and Description |
---|---|
AnchorPoint |
QualifySketchBuilder.createNewAnchorPoint()
Creates the anchor point.
|
AnchorPoint |
AnchorPointList.findItem(int index)
Returns the object at the input index.
|
AnchorPoint[] |
AnchorPointList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
AnchorPointList.append(AnchorPoint object)
Appends an object to the list
License requirements: None. |
void |
AnchorPointList.append(AnchorPoint[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
AnchorPointList.erase(AnchorPoint obj)
Erases the object from the list, but does not delete the object.
|
void |
AnchorPointList.erase(AnchorPoint obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
AnchorPointList.findIndex(AnchorPoint obj)
Finds the index where the input object appears.
|
void |
AnchorPointList.insert(int location,
AnchorPoint object)
Inserts an object at the specified location
License requirements: None. |
void |
AnchorPointList.setContents(AnchorPoint[] objects)
Sets the contents of the entire list.
|
void |
AnchorPointList.swap(AnchorPoint object1,
AnchorPoint object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.