Package | Description |
---|---|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
Modifier and Type | Field and Description |
---|---|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
AlongGuideCutBuilder.WaterStopOffsetMethod.ASYMMETRIC
The left offset and right offset are asymmetric
|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
AlongGuideCutBuilder.WaterStopOffsetMethod.SYMMETRIC
The left offset and right offset are symmetric
|
Modifier and Type | Method and Description |
---|---|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
AlongGuideCutBuilder.WaterStopOffsetMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlongGuideCutBuilder.WaterStopOffsetMethod |
AlongGuideCutBuilder.WaterStopOffsetMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlongGuideCutBuilder.WaterStopOffsetMethod[] |
AlongGuideCutBuilder.WaterStopOffsetMethod.values()
Returns an array that contains the values for this enum.
|
AlongGuideCutBuilder.WaterStopOffsetMethod |
AlongGuideCutBuilder.waterStopOffsetOption()
Returns the offset option when the
AlongGuideCutBuilder.CreationMethod
is AlongGuideCutBuilder.CreationMethod.WATER_STOP . |
Modifier and Type | Method and Description |
---|---|
void |
AlongGuideCutBuilder.setWaterStopOffsetOption(AlongGuideCutBuilder.WaterStopOffsetMethod offsetOption)
License requirements: nx_ship_detail ("Ship Detail Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.