public static class StiffenerBuilder.AttachmentOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INFERRED
Infer the plate on which to attach the stiffener
|
static int |
_OVERRIDE
Use the selected attachment plate on which to attach the stiffener
|
static StiffenerBuilder.AttachmentOption |
INFERRED
Infer the plate on which to attach the stiffener
|
static StiffenerBuilder.AttachmentOption |
OVERRIDE
Use the selected attachment plate on which to attach the stiffener
|
Modifier and Type | Method and Description |
---|---|
static StiffenerBuilder.AttachmentOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StiffenerBuilder.AttachmentOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StiffenerBuilder.AttachmentOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final StiffenerBuilder.AttachmentOption INFERRED
public static final StiffenerBuilder.AttachmentOption OVERRIDE
public static final int _INFERRED
public static final int _OVERRIDE
public static StiffenerBuilder.AttachmentOption valueOf(int value)
public static StiffenerBuilder.AttachmentOption valueOf(String name)
public static StiffenerBuilder.AttachmentOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.