public static class HemFlangeBuilder.InsetTypeOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BEND_OUTSIDE
The bend and hem flange are outside the thickness face
|
static int |
_MATERIAL_INSIDE
The hem flange is flush with the thickness face on the inside
|
static int |
_MATERIAL_OUTSIDE
The hem flange is flush with the thickness face on the outside
|
static HemFlangeBuilder.InsetTypeOptions |
BEND_OUTSIDE
The bend and hem flange are outside the thickness face
|
static HemFlangeBuilder.InsetTypeOptions |
MATERIAL_INSIDE
The hem flange is flush with the thickness face on the inside
|
static HemFlangeBuilder.InsetTypeOptions |
MATERIAL_OUTSIDE
The hem flange is flush with the thickness face on the outside
|
Modifier and Type | Method and Description |
---|---|
static HemFlangeBuilder.InsetTypeOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HemFlangeBuilder.InsetTypeOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HemFlangeBuilder.InsetTypeOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final HemFlangeBuilder.InsetTypeOptions MATERIAL_INSIDE
public static final HemFlangeBuilder.InsetTypeOptions MATERIAL_OUTSIDE
public static final HemFlangeBuilder.InsetTypeOptions BEND_OUTSIDE
public static final int _MATERIAL_INSIDE
public static final int _MATERIAL_OUTSIDE
public static final int _BEND_OUTSIDE
public static HemFlangeBuilder.InsetTypeOptions valueOf(int value)
public static HemFlangeBuilder.InsetTypeOptions valueOf(String name)
public static HemFlangeBuilder.InsetTypeOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.