public static class BridgeTransitionBuilder.WidthOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FINITE
Bridge Transition starts at specified point on start edge and extends on one side by the specified distance.
|
static int |
_FULL_BOTH_EDGES
Bridge Transition spans the full length of both the edges.
|
static int |
_FULL_END_EDGE
Bridge Transition spans the full length of end edge.
|
static int |
_FULL_START_EDGE
Bridge Transition spans the full length of start edge.
|
static int |
_SYMMETRIC
Bridge Transition starts at specified point on start edge and extends on either side by half the specified distance.
|
static BridgeTransitionBuilder.WidthOptions |
FINITE
Bridge Transition starts at specified point on start edge and extends on one side by the specified distance.
|
static BridgeTransitionBuilder.WidthOptions |
FULL_BOTH_EDGES
Bridge Transition spans the full length of both the edges.
|
static BridgeTransitionBuilder.WidthOptions |
FULL_END_EDGE
Bridge Transition spans the full length of end edge.
|
static BridgeTransitionBuilder.WidthOptions |
FULL_START_EDGE
Bridge Transition spans the full length of start edge.
|
static BridgeTransitionBuilder.WidthOptions |
SYMMETRIC
Bridge Transition starts at specified point on start edge and extends on either side by half the specified distance.
|
Modifier and Type | Method and Description |
---|---|
static BridgeTransitionBuilder.WidthOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeTransitionBuilder.WidthOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeTransitionBuilder.WidthOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeTransitionBuilder.WidthOptions FINITE
public static final BridgeTransitionBuilder.WidthOptions SYMMETRIC
public static final BridgeTransitionBuilder.WidthOptions FULL_START_EDGE
public static final BridgeTransitionBuilder.WidthOptions FULL_END_EDGE
public static final BridgeTransitionBuilder.WidthOptions FULL_BOTH_EDGES
public static final int _FINITE
public static final int _SYMMETRIC
public static final int _FULL_START_EDGE
public static final int _FULL_END_EDGE
public static final int _FULL_BOTH_EDGES
public static BridgeTransitionBuilder.WidthOptions valueOf(int value)
public static BridgeTransitionBuilder.WidthOptions valueOf(String name)
public static BridgeTransitionBuilder.WidthOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.