Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static LocalOffsetBuilder.ShapeMethodType |
LocalOffsetBuilder.ShapeMethodType.SHARP
Sharp specifies a transition region without smoothing.
|
static LocalOffsetBuilder.ShapeMethodType |
LocalOffsetBuilder.ShapeMethodType.SMOOTH
Smooth specifies a transition region with smoothing.
|
Modifier and Type | Method and Description |
---|---|
LocalOffsetBuilder.ShapeMethodType |
LocalOffsetBuilder.shapeMethod()
Returns the method to define the shape of the transition region
License requirements: None. |
static LocalOffsetBuilder.ShapeMethodType |
LocalOffsetBuilder.ShapeMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LocalOffsetBuilder.ShapeMethodType |
LocalOffsetBuilder.ShapeMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LocalOffsetBuilder.ShapeMethodType[] |
LocalOffsetBuilder.ShapeMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LocalOffsetBuilder.setShapeMethod(LocalOffsetBuilder.ShapeMethodType shapeMethod)
License requirements: nx_polygon_modeling (" NX Polygon Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.