Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.CleanupOptions.ANALYZE
Perform Analysis
|
static CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.CleanupOptions.NONE
Don't perform Analysis or Repair
|
static CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.CleanupOptions.REPAIR
Perform Repair
|
Modifier and Type | Method and Description |
---|---|
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.foldedEdges()
Returns the option to identify or repair facets having an angle with adjacent facets less than a specified minimum value
License requirements: None. |
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.inconsistentNormals()
Returns the option to identify or repair normals of neighboring facets or vertices that do not have the right orientation
License requirements: None. |
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.laminarSlits()
Returns the option to identify or repair thin holes or slits in the mesh caused by facets not being aligned
License requirements: None. |
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.longFacets()
Returns the option to identify or repair facets with a ratio of longest to shortest side exceeding a specified value
License requirements: None. |
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.selfIntersections()
Returns the option to identify or repair facets of the same mesh intersecting each other
License requirements: None. |
CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.thinFacets()
Returns the option to identify or repair facets with with one long edge and two edges with more or the less the same length and a ratio of length to width exceeding a specified value
License requirements: None. |
static CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.CleanupOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CleanupFacetBodyBuilder.CleanupOptions |
CleanupFacetBodyBuilder.CleanupOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CleanupFacetBodyBuilder.CleanupOptions[] |
CleanupFacetBodyBuilder.CleanupOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CleanupFacetBodyBuilder.setFoldedEdges(CleanupFacetBodyBuilder.CleanupOptions foldedEdges)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
CleanupFacetBodyBuilder.setInconsistentNormals(CleanupFacetBodyBuilder.CleanupOptions inconsistentNormals)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
CleanupFacetBodyBuilder.setLaminarSlits(CleanupFacetBodyBuilder.CleanupOptions laminarSlits)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
CleanupFacetBodyBuilder.setLongFacets(CleanupFacetBodyBuilder.CleanupOptions longFacets)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
CleanupFacetBodyBuilder.setSelfIntersections(CleanupFacetBodyBuilder.CleanupOptions selfIntersections)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
CleanupFacetBodyBuilder.setThinFacets(CleanupFacetBodyBuilder.CleanupOptions thinFacets)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.